MEAN WELL Introduced High Power and Horticultural Lighting Solution at SIL show 2018

    Long Beach, California, Feb 13-15, 2018 – MEAN WELL presented its latest LED Power solutions at Strategies In Light, The LED show, (SIL), Long Beach, 2018. As one of the leading LED show in North America, SIL show attracted more than 5000 attendees from 60 countries, with the latest trend and technologies shaping the future in LED industry.

   MEAN WELL exhibited its extension range of the latest LED power solution, such as the HLG (C.V.+C.C. output) and HLG-C (C.C. output) series, the most outstanding models of high performance LED drivers in the LED lighting industry. MEAN WELL is also delighted to unveil the new 480W- 600W series: HLG-480H and HLG-480H-C, HVG-480H, HVGC-480 and HLG-600H in order to meet the booming market demand from High Bay and Horticultural Lighting; also suitable for stadium and flood Lighting. MEAN WELL will also soon release new constant power mode HVGC-650 series, which is targeted for high power, wide range adjustable constant current LED market. Please check www.meanwellusa.com for more product detail.