MEAN WELL acquired the UL458 (Power converters & inverters and power converter & inverter systems for land vehicles and marine crafts) certificate for its F-type model (with GFCI output socket) of TN-1500, TS-1500, and TS-1000 series DC/AC true sine wave inverters. Along with E13 and CE, these true sine wave inverters can fulfill the requirements of different applications for most of the countries and areas in the world.
In the mean time, in response to the demand of end users, MEAN WELL also changed the factory setting of TN-1500 from “energy saving mode” to “UPS mode”. If needed, users can still easily select these two operation modes through the setting button on the front panel or the monitoring software to achieve the optimal system design.