Powered by MEAN WELL


MEAN WELL Premium Partner Zone

Learn More

Client Testimonial


About Yuanhui


Cixi Yuanhui Lighting Electric Co.,Ltd. located in Sanbei lndustry Area,SanBei Town, Cixi ity, Ningbo, China, covering an area of 16000 square meters. It benefits itself with convenient traffic: about 40 minutes’ drive to Ningbo Airport, 45 minutes to Ningbo Port, 2 hours to arrive in Shanghai and only 30 minutes to Hangzhou Bay Bridage-----the world’s longest bridage.

Yuanhui’s new working areas are equipped with injection, gear tray stamping and coating, lighting components, assemble line etc. With these equipments, Yuanhui has obtained the capacity of producing 3 million sets of lighting fixtures. Yuanhui provides products and services strictly in accordance with ISO9001 and CE,GS standards. Yuanhui has passed and got relative certive certificates. With its goal to be one of the most professionals manufactures of IP65 fluorescent lighting fixtures, Yuanhui konows well the innovation is the primary source of their energy.

Yuanhui has developed its T8/T5 series IP65 fluoresecent lights, and has waterproof, dustproof, humidity proof function.

For more information, please refer to Yuanhui website(http://www.cxyuanhui.com)。